SLVSGY2A October 2023 – October 2025 TPS2HCS10-Q1
PRODUCTION DATA
When a thermal shutdown or an overcurrent protection fault occurs, the channel with the fault will either auto-retry or latch off based on the LATCH_CHx bit setting in the CHx_CONFIG registers. Depending on the CAP_CHRG_CHx settings the auto retry response will behave differently.
Note, in LIMP_HOME state the device will continuously retry regardless of the LATCH_CHx setting if the channel is configured to be ON in LIMP_HOME state through the CHx_LH_IN bits. The retry behavior in LIMP_HOME state will follow the below sections depending on how the CAP_CHRG_CHx bits are configured.
If CAP_CHRG_CHx = 00 and LATCH_CHx = 0 and a short circuit event occurs, after the channel turns off and tRETRY expires the device will retry in the inrush period with the IOCP level set through the INRUSH_LIMIT_CHx [3:0] bits. The INRUSH_DURATION_CHx [2:0] still sets the duration of the inrush period. Figure 8-8 showcases this hot short case that occur in steady state operation. Starting into a short in the inrush period results in the same retry behavior as a hot short in steady state except the first initial overcurrent shutdown level will be determined by the INRUSH_LIMIT_CHx [3:0].
If LATCH_CHx = 1 and CAP_CHRG_CHx = 00 and the IOCP level is exceeded, the device will latch-off and will not retry until the CHx_ON bit (version A) is toggled or the DIx pin (version B) is toggled or the LATCH_CHx bit is toggled. Upon resetting the latch either through an output toggle or through the LATCH_CHx bit toggle, the channel will start up into the inrush period if configured. Figure 8-9 below shows the latch behavior if a hot short circuit occurs during steady state operation with LATCH_CHx = 1. Figure 8-10 shows the latch behavior if the channel starts into a short circuit event in the inrush period.
If a short circuit event occurs in steady state operation with CAP_CHRG_CHx = 10 and LATCH_CHx = 0, after the channel turns off and tRETRY expires the device will retry into the inrush period with the current limit regulation (ICL_REG) set through the INRUSH_LIMIT_CHx [3:0] bits. Figure 8-11 shows a hot short event that occurs in steady state operation with CAP_CHRG_CHx = 10 and LATCH_CHx = 0. Figure 8-12 shows the auto-retry behavior if the channel starts into a short circuit event in the inrush period.
If LATCH_CHx = 1 and CAP_CHRG_CHx = 10 and the IOCP level is exceeded, the device will latch-off and will not retry until the CHx_ON bit (version A) is toggled or the DIx pin (version B) is toggled or the LATCH_CHx bit is toggled. Upon resetting the latch either through an output toggle or through the LATCH_CHx bit toggle, the channel will start up into the inrush period if configured. Figure 8-13 below shows the latch behavior if a hot short circuit occurs during steady state operation with LATCH_CHx = 1. Figure 8-14 shows the latch behavior if the channel starts into a short circuit event in the inrush period.