SLVUCU5 December 2025 UCD91160 , UCD91320
The RESTORE_DEFAULT_ALL command restores the PMBus parameters from the Default Store into Operating Memory. If the Default Store has never been written, values from the hard-coded memory are used.
This command is not supported on UCD91xxx.
Resetting the device is a better (more thorough) way to perform this operation.