SLVUCU5 December 2025 UCD91160 , UCD91320
The device verifies the firmware by using a checksum algorithm at each power up. If the checksum does not match, the device resets. If the device continues to reset, the SYNC_CLK pin outputs repeated pulses with an approximate 250-ms pulse width that can be observed externally.
The device performs a configuration checksum verification at power up. If the checksum does not match, the device discards all the configuration data. The PMBALERT pin is asserted and a flag is set in the status register.
A fault-log checksum verification in Flash is also performed at power up. Each log entry has a checksum. The device ignores the corrupted log entries.