SLVUCU5 December 2025 UCD91160 , UCD91320
Each page has its own GPO Sequence On Dependency Mask, whose bits are defined in the following table:
| Bit | 15 | ... | 5 | 4 | 3 | 2 | 1 | 0 |
|---|---|---|---|---|---|---|---|---|
| Purpose | GPO16 | ... | GPO6 | GPO5 | GPO4 | GPO3 | GPO2 | GPO1 |
It is logical state selected by the GPO not the actual pin output of the GPO used as dependency.
The enable pin for the page is not deasserted until all of the logical states selected by the GPO bits are FALSE. Once the enable pin is deasserted, the logical state of these GPO has no effect on the state of the enable pin.
Each page can depend on the state of up to 16 GPO logical states. The same states can be used to control multiple pages (see Section 26.38).