SLVUD83A July 2025 – September 2025
The register map page lists the different registers available for configuration and is intended for direct reads and writes to the PMIC registers, as shown in Figure 3-7. Reading and writing registers are either done individually or all at once. Enable the Auto Read feature by using the drop-down menu next to the READ ALL REGISTERS button to select an automatic read timing. Use the search bar at the top of the page to search registers by name or address.
The first three columns under the search bar show the name of each register, followed by the hexadecimal address and data value. The Bits column contains the bit values for each register and can be hidden by unchecking the Show Bits box at the top of the page, under the READ ALL REGISTERS button. Double-clicking a bit in this section changes the bit value.
The Field View section on the right side of the page shows register bits grouped by the respective control blocks. Click on any bit field box to see the corresponding bits highlighted in yellow in the Bits column. Each field has a name shown by the blue text at the top of each box. Find these names using the search bar by checking the Search Bitfields box (next to Show Bits).
In the Immediate Write mode (drop-down option located at the top right of the page), write buttons are grayed out since individual registers are written immediately with each change in the Field View, change in bits, or change in hexadecimal value. In Deferred Write mode, the writing of a single register or all registers is deferred until the WRITE REGISTER or WRITE ALL REGISTERS button is selected.
Figure 3-7 Register Map Page