Configure the TPS65215Q1EVM as follows. The following sections outline how to configure the TPS65215Q1EVM for general experimentation.
- Configure regulator input supply rails for the expected application using the jumpers indicated in the Supply Voltage Setup.
- Configure the multi-function pins externally using the mode configuration descriptions indicated in ulti-Function Pin Setup. Please note that the default configuration for regulator choice in SD or DDR voltage selection differs for each individual NVM configuration (polarity is configurable).
- Connect VSYS to a power supply capable of supporting the application and enable the supply.
- If using a version of TPS65215-Q1 configured for first supply detection (FSD), then the power-up sequence is executed as soon as a valid supply is connected to VSYS.