Below instructions are for the Code Composer Studio IDE.
- Install Code Composer Studio (CCS) and the MSPM0 SDK.
- After installation open CCS and navigate to the top left, then select "File"
- Select Import Projects
- Click browse then navigate to the MSPM0 SDK
install, the default path is C:\ti\mspm0_sdk_x_xx_xx_xx, where x is the version
number.
- Navigate through examples > nortos >
LP_MSPM0G3708 > riverlib, and click on
gpio_toggle_output then select folder
- Click on the ticlang version of the example and
click finish, then the example is imported.
- Plug in the LP-MSPM0G3708 into the PC with a USB cable
- Right click on the gpio_toggle_output example and
select "debug project" or "flash project", this action starts the programming of the
device.
- Once flashed, run the program and observe the flashing lights on the board.
Explore any additional code examples and the .sysconfig file to start development.