SNVSC77B December 2024 – April 2025 LM5125-Q1
PRODUCTION DATA
The device integrates N-channel logic MOSFET drivers. The LOx driver is powered by VCC and the HOx driver is powered by HBx. When the SWx-pin voltage is approximately 0V by turning on the low-side MOSFET, the capacitor CHBx is charged from VCC through the internal boot diode. The recommended value of CHBx is 0.1μF. During shutdown, the gate drivers outputs are high impedance.
The LOx and HOx outputs are controlled with an adaptive dead-time methodology, which makes sure that both outputs are not turned on at the same time to prevent shoot through. When the device turns on LOx the adaptive dead-time logic turns off HOx and waits for the HOx-SWx voltage to drop below typically 1.5V, then LOx is turned on after a small programmable dead-time delay tDHL. Also the HOx driver turn-on is delayed until the LOx-PGND voltage has discharged below typically 1.5V. HOx is then turned on after the same programmable dead-time delay tDLH.
If the driver output voltage is lower than the MOSFET gate plateau voltage during start-up, the converter cannot start up properly and can be stuck at the maximum duty cycle in a high-power dissipation state. Avoid this condition by selecting a lower threshold MOSFET or by turning on the device when the BIAS-pin voltage is sufficient. During bypass operation the minimum HOx − SWx voltage is 3.75V.
The hiccup mode fault protection is triggered by VHB-UVLO. If the HBx − SWx voltage is less than the HBx UVLO threshold (VHB-UVLO), LOx turns on by force for 75ns to replenish the boost capacitor. The device allows up to four consecutive replenish switching cycles. After the maximum four consecutive boot replenish switching cycles, the device skips switching for 12 cycles. If the device fails to replenish the boost capacitor after the four sets of the four consecutive replenish switching cycles, the device stops switching and enters 512 cycles of hiccup mode off-time. During the hiccup mode off-time PGOOD = low and the SS-pin is grounded.
If required adjust the slew rate of the switching node voltage by adding a gate resistor in parallel with pull-down PNP transistor. The resistor decreases the effective dead-time.
Figure 6-18 Slew Rate Control