SPNU118Z September 1995 – March 2023 66AK2E05 , 66AK2H06 , 66AK2H12 , 66AK2H14 , AM1705 , AM1707 , AM1802 , AM1806 , AM1808 , AM1810 , AM5K2E04 , OMAP-L132 , OMAP-L137 , OMAP-L138 , SM470R1B1M-HT , TMS470R1A288 , TMS470R1A384 , TMS470R1A64 , TMS470R1B1M , TMS470R1B512 , TMS470R1B768
Initialize Field
.fieldvalue[, size in bits]
The .field directive initializes a multiple-bit field within a single word (32 bits) of memory. This directive has two operands:
*** WARNING! line 21: W0001: Field value truncated to 1
.field 3, 1Successive .field directives pack values into the specified number of bits starting at the current word. Fields are packed starting at the most significant part of the word, moving toward the least significant part as more fields are added. If the assembler encounters a field size that does not fit into the current word, it writes out the word, and begins packing fields into the next word.
The .field directive is similar to the .bits directive (see the .bits topic). However, the .bits directive does not force alignment to a field boundary and does not automatically increment the SPC when a word boundary is reached.
Use the .align directive to force the next .field directive to begin packing a new word.
If you use a label, it points to the byte that contains the specified field.
When you use .field in a .struct/.endstruct sequence, .field defines a member's size; it does not initialize memory. For more information, see the .struct/.endstruct/.tag topic.
This example shows how fields are packed into a word. The SPC does not change until a word is filled and the next word is begun.
1 ************************************
2 ** Initialize a 14-bit field. **
3 ************************************
4 00000000 2AF00000 .field 0ABCh, 14
5
6 ************************************
7 ** Initialize a 5-bit field **
8 ** in the same word. **
9 ************************************
10 00000000 2AF14000 L_F: .field 0Ah, 5
11
12 ************************************
13 ** Write out the word. **
14 ************************************
15 .align 4
16
17 ************************************
18 ** Initialize a 4-bit field. **
19 ** This fields starts a new word. **
20 ************************************
21 00000004 C0000000 x: .field 0Ch, 4
22
23 ************************************
24 ** 32-bit relocatable field **
25 ** in the next word. **
26 ************************************
27 00000008 00000004' .field x
28
29 ************************************
30 ** Initialize a 32-bit field. **
31 ************************************
32 0000000c 00004321 .field 04321h, 32
Figure 5-6 shows how the directives in this example affect memory.
Figure 5-6 The .field
Directive