SPRAC94D September   2018  – March 2022 AFE030 , AFE031 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S

 

  1.   Trademarks
  2. 1 FSK Overview
  3. 2 Hardware Overview
    1. 2.1 Block Diagram
    2. 2.2 Hardware Setup
  4. 3 Interfacing With the AFE03x
    1. 3.1 Configuring the AFE031
  5. 4 Transmit Path
    1. 4.1 FSK Example Specifications
    2. 4.2 PWM Mode
      1. 4.2.1 Software Implementation
      2. 4.2.2 Testing Results
      3. 4.2.3 HRPWM vs. EPWM
    3. 4.3 DAC Mode
      1. 4.3.1 Software Implementation
      2. 4.3.2 Testing Results
      3. 4.3.3 OFDM Ability
    4. 4.4 Porting TX to LAUNCHXL-F280049C
      1. 4.4.1 PWM Mode Specific Porting
      2. 4.4.2 DAC Mode Specific Porting
  6. 5 Receive Path
    1. 5.1 Receive Path Overview
    2. 5.2 Receiver Software Implementation
      1. 5.2.1 Initial Setup and Parameters
      2. 5.2.2 Interrupt Service Routines
      3. 5.2.3 Run Time Operation
      4. 5.2.4 Testing Results
      5. 5.2.5 System Utilization
      6. 5.2.6 Device Dependency and Porting
    3. 5.3 Tuning and Calibration
      1. 5.3.1 Setting the AFE03X's PGAs
      2. 5.3.2 Automatic Gain Control (AGC)
      3. 5.3.3 Setting the Bit Detection Threshold
      4. 5.3.4 FSK Correlation Detector Library
    4. 5.4 Porting RX to LAUNCHXL-F280049C
  7. 6 Interfacing With a Power Line
    1. 6.1 Line Coupling
    2. 6.2 Coupling to an AC Line
      1. 6.2.1 Low Voltage Capacitor
      2. 6.2.2 The Ratio of the Transformer
      3. 6.2.3 HV Capacitor
      4. 6.2.4 HV Side Inductor
    3. 6.3 Coupling to DC Line
    4. 6.4 Protection Circuit
      1. 6.4.1 Metal Oxide Varistors
      2. 6.4.2 Transient Voltage Suppressors
      3. 6.4.3 Current Steering Diodes
    5. 6.5 Determining PA Power Supply Requirements
  8. 7 Summary
  9. 8 References
  10. 9 Schematics
    1. 9.1 Schematics (PWM Mode)
    2. 9.2 Schematics (DAC Mode)
  11. 10Revision History

Testing Results

The performance of the FSK receiver solution was tested in a controlled lab environment using either the PWM or DAC mode transmitter solution to provide the input FSK signal. The established setup is similar to what is shown in Figure 2-8 without any coupling circuitry. The purpose of the tests were to confirm that the receiver solution could effectively translate a received FSK signal into the original digital information.

When the guidelines discussed in Section 5.2 are appropriately followed, a C2000 MCU can take a FSK input signal and accurately decode each bit of data it contains. This is shown in Figure 5-5, where a packet of thirty-three unique bits were successfully captured.

GUID-160712B0-9ECE-4088-AD6F-110D9D0F7F34-low.gifFigure 5-5 Packet of Recieved Bits of Data

This captured data is in the form of an 11-bit code word transmitted three consecutive times. Each code word having a sum of one is then packetized in the format shown in Figure 5-6

GUID-CC54E8CA-BA18-4C0E-BD48-1676F90A2CFD-low.gifFigure 5-6 Packetized Data