SPRACZ7 January   2022 TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28232 , TMS320F28232-Q1 , TMS320F28234 , TMS320F28234-Q1 , TMS320F28235 , TMS320F28235-Q1 , TMS320F28332 , TMS320F28333 , TMS320F28334 , TMS320F28335 , TMS320F28335-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S

 

  1.   Trademarks
  2. 1 Introduction
    1. 1.1 Abbreviations
  3. 2 Central Processing Unit (CPU)
  4. 3 Development Tools
    1. 3.1 Driver Library (Driverlib)
    2. 3.2 Embedded Application Binary Interface (EABI) Support
  5. 4 Package and Pinout
  6. 5 Operating Frequency and Power Management
  7. 6 Power Sequencing
  8. 7 Input Clock Options
  9. 8 Memory Map
  10. 9 Flash and OTP
    1. 9.1 Size and Number of Sectors
    2. 9.2 Flash Parameters
    3. 9.3 Flash Programming
    4. 9.4 Entry Point into Flash
    5. 9.5 Dual Code Security Module (DCSM) and Password Locations
    6. 9.6 OTP
  11. 10Boot ROM
    1. 10.1 Boot ROM Reserved RAM
    2. 10.2 Boot Mode Selection
    3. 10.3 Bootloaders
  12. 11Architectural Enhancements
    1. 11.1 Clock Sources and Domains
    2. 11.2 Watchdog Timer
    3. 11.3 Peripheral Interrupt Expansion (PIE)
    4. 11.4 Lock Protection Registers
    5. 11.5 General-Purpose Input/Output (GPIO)
    6. 11.6 External Interrupts
    7. 11.7 Crossbar (X-BAR)
  13. 12Peripherals
    1. 12.1 New Peripherals
      1. 12.1.1 Analog Subsystem Interconnect
      2. 12.1.2 Comparator Subsystem (CMPSS)
      3. 12.1.3 Control Law Accelerator (CLA)
    2. 12.2 Control Peripherals
      1. 12.2.1 Enhanced Pulse Width Modulator (ePWM)
      2. 12.2.2 Enhanced Capture Module (eCAP)
      3. 12.2.3 Enhanced Quadrature Encode Pulse Module (eQEP)
      4. 12.2.4 Sigma-Delta Filter Module (SDFM)
    3. 12.3 Analog Peripherals
      1. 12.3.1 Analog-to-Digital Converter (ADC)
    4. 12.4 Communication Peripherals
      1. 12.4.1 SPI
      2. 12.4.2 SCI
      3. 12.4.3 USB
      4. 12.4.4 I2C
      5. 12.4.5 CAN
  14. 13Configurable Logic Block (CLB)
  15. 14Device Comparison Summary
  16. 15References

Crossbar (X-BAR)

The X-BARs provide a flexible means for interconnecting multiple inputs, outputs, and internal resources in various configurations. The F2837xD/S/07x devices contains three X-BARs: the Input X-BAR, the Output X-BAR, and the ePWM X-BAR.

  • Input X-BAR – is used to route external GPIO signals into the device. It has access to every GPIO pin where each signal can be routed to any or multiple destinations which include the ADCs, eCAPs, ePWMs, Output X-BAR, and external interrupts. The F2837xD/S/07x Input X-BAR has fourteen inputs (INPUT1 through INPUT14) and INPUT7 through INPUT12 can be selected as an external input to each of the eCAP modules.
    Note:

    This differs from the F2833x/23xdevices which uses the GPIO multiplexer to select a specific dedicated input pin to access the eCAP module.

  • Output X-BAR – is used to route various internal signals out of the device. It contains eight outputs that are routed to the GPIO structure, where each output has one or multiple assigned pin positions, which are labeled as OUTPUTXBARx. Additionally, the Output X-BAR can select a single signal or logically OR up to 32 signals.
  • ePWM X-BAR – is used to route signals to the ePWM Digital Compare submodules of each ePWM module for actions such as trip zones and synchronizing. It contains eight outputs that are routed as TRIPx signals to each ePWM module. Likewise, the ePWM X-Bar can select a single signal or logically OR up to 32 signals.