SPRZ530B april 2022 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
USB: 2.0 Compliance Receive Sensitivity Test
Limitation
Performing receive sensitivity tests (EL_16 and EL_17) as defined in the USB-IF USB 2.0 Electrical Compliance Test Specification may invoke the problem described in Advisory i2091.
The issue was originally found while performing these tests using automation software, which increased USB signal amplitude while sending packets. The software was sweeping the amplitude from a value less than 100 mV to a value greater than 150 mV while verifying the device under test (DUT) NAK’d all packets below 100 mV and NAK’d no packets above 150 mV. However, increasing the amplitude through the squelch threshold while sending valid packets may lock the PHY as described in Advisory i2091.
Enable both of the following hardware workarounds.
Set cdr_eb_wr_reset bit (bit 7) to 1’b1 in UTMI_REG28 register present in USB*_PHY2 region.
Set phyrst_a_enable bit (bit 0) to 1’b1 in PHYRST_CFG register present in USB*_MMR_MMRVBP_USBSS_CMN region. Please note that phyrst_a_value (bits 12:8) in PHYRST_CFG register should be retained at default value of 0xE.