SPRZ530B april 2022 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
DDR: Controller Anomaly in Setting Wakeup Time for Low Power
States
The DDR controller may erroneously decrease the wakeup time for the present low power state if the wakeup time for the next deeper power state is either disabled, or set to a lower value.
If a particular low power state is enabled by setting a bit in the DDRSS_CTL_139[29-24] LPI_WAKEUP_EN bit field, all deeper power state bits must also be enabled. From bit 0 through 4, low power states go deeper and deeper as the bit number increases. For example, if bit 0 is set, all bits from 1 through 4 must also be set. Similarly, if bit 2 is set, bit 3 and 4 must also be set.
In addition, the following wakeup values must be programmed in increasing order:
where FN = F0, F1, and F2 for different frequency set points.