SPRZ530B april 2022 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
UDMA: Force teardown bitfield readback is masked in realtime TX/RX registers
The force teardown bit field will not remain set in the read back of the realtime TX/RX registers after a force teardown is initiated.
The Force Teardown operation is only used by software to intervene to address a catastrophic system condition, so software should separately track when it initiates a forced teardown verses a normal teardown, and thus not depend on the readback value of the force teardown bitfield to obtain this information.