SPRZ530B april 2022 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
GPMC: Sub-32-bit read issue with NAND and FPGA/FIFO
Sub-32-bit reads on the GPMC interface will miss portions of the data, which will result in incorrect read data. This includes 8-bit or 16-bit reads from a NAND device or from an FPGA or FIFO interface. Note that 3-byte accesses are not allowed on the GPMC interface.
Read accesses on the GPMC interface must be performed as 32-bit reads. Writes are not affected by this erratum.