SPRZ530B april 2022 – june 2023 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
Restrictions on how CP Tracer Debug Probes can be used
Some CP Tracer bus probes do not receive the full SoC physical address but only a minimal set that was relevant to endpoint being monitored. This limits the usefulness of the probe in the SoC Analysis > Traffic Profiling feature in CCS.
1) Address Filtering / Matching : User would typically input the full 36b/40b (depending on device) address for any address-qualified bus probe jobs.
2) Decoding of transaction trace : User would expect that the address provided in the decoded stream was the full 36b/40b physical address of the transaction.
Affected probes:
J7AEP: SoC Onchip SRAM, MCU FlashSS
none