STDA039 July 2026 F28377D-SEP , INA901-SP , SN54SLC8T245-SEP , TPS7A4501-SP , TPS7H1121-SEP , TPS7H1121-SP , TPS7H5020-SEP , TPS7H5020-SP , TPS7H6101-SEP
When a COTS or automotive component is sourced for space applications, the preferred strategy is to buy sufficient material from a single lot. In practice, however, manufacturers often spread production across multiple wafer fabs and assembly sites. Each fab potentially uses slightly different equipment, process settings, or material recipes, and each assembly plant can employ distinct mold compounds and bond‑wire materials. While these variations normally have no effect on performance as long as the part operates within the datasheet limits, these variations can become critical when the component is pushed beyond those limits, especially under the harsh radiation environment of space.
Figure 3-1 Transistor Voltage Thresholds Over
Multi-Lot Variations Together With Expected Drifts from Radiation (TID) Can Significantly
Compromise the Life Cycle in Space for a Single UnitIf a space program purchases parts from a possibly mixed lot, the lot qualification or testing can potentially differ from the lot that is used for launch, creating a hidden reliability risk. Even more problematic is the situation where a design that has proven successful in flight must be scaled up to meet growing demand. New production lots can incorporate process optimizations, different materials, or design tweaks aimed at improving yield and reducing cost. Those changes can degrade the very radiation hardness or reliability that the original lot exhibited, so the new lots potentially no longer pass the original qualification. Over time, this risk grows because suppliers continually refine processes, and the original flight‑heritage configuration can become unavailable. The consequence is, that a component, board or module, that has accumulated years of flight heritage potentially needs to be redesigned and requalified or delta-qualified, if the exact original version can no longer be sourced, thereby the heritage value is lost.
Automotive parts, in particular, are produced in very high volumes and are subject to frequent cost‑ and yield‑driven changes, often requiring multiple fabrication pathways to maintain supply resilience. Due to the constant evolution of these parts, these parts can actually be poorer candidates for up‑screening into space applications, where stability and traceability of the manufacturing process are essential. The risks outlined above can be addressed through one of two approaches: either investing in an assured production run from a single wafer or lot—which carries potential additional costs—or accepting the inherent risk by procuring a complete component reel on the assumption of homogeneous production.
Figure 3-2 Space-Grade Products from TI, Including
Space EP (SEP) Products Follow a Single Baseline Controlled FlowThus, establishing a single, controlled baseline—by fixing the wafer fab, assembly site, and material set (including mold compound and bond‑wire type) plus performing a radiation lot acceptance test (RLAT) for every new lot produced—is essential so that every part used in a space system matches the qualified unit, thereby preserving reliability and heritage throughout the life cycle of the program.
Figure 3-3 Quality Assurance (QA) is a Systematic
Process from the Ground-Up