STDA039 July   2026 F28377D-SEP , INA901-SP , SN54SLC8T245-SEP , TPS7A4501-SP , TPS7H1121-SEP , TPS7H1121-SP , TPS7H5020-SEP , TPS7H5020-SP , TPS7H6101-SEP

 

  1.   1
  2.   Abstract
  3. 1Introduction
  4. 2Space ‑ Electronics Design Landscape
  5. 3Importance of a Single Controlled Baseline
  6. 4The Steps to Take to Upscreen a COTS Device
    1. 4.1 Step 1 – Identifying the Candidates
    2. 4.2 Step 2 – Preparation for Single‑Event Effect (SEE) Testing (Opening)
    3. 4.3 Step 3 – Single‑Event Effect (SEE) Testing
    4. 4.4 Step 4 – Running TID Tests and Evaluating Radiation Lifetime
  7. 5Lead‑Time and Yield Responsibility
  8. 6Summary
  9. 7References

Introduction

The rise of commercial space services is accelerating the launch of low Earth orbit (LEO) constellations, while deep space, MEO (medium Earth orbit), and GEO (geostationary Earth orbit) missions still require the utmost reliability over long lifetimes; designers therefore contend with two opposing goals—minimizing cost versus maximizing reliability—pursued through the new space approach (cost focused LEO constellations) and the traditional space approach (risk focused deep space, MEO and GEO satellites).

Up screening commercial off the shelf (COTS) components can potentially lower bill of materials (BOM) costs for high volume LEO constellations, but the practice creates a distinct risk profile that must be quantified and mitigated. In contrast, space qualified parts deliver deterministic performance in the harsh space environment, often accompanied by proven flight heritage. These parts are typically the only viable option for longer duration missions that cannot tolerate any risk—such as MEO and GEO satellites, which must achieve extended lifetimes to amortize high launch costs and endure increased radiation from permanent proximity to the Van Allen belts—as well as deep space and legacy programs, albeit at a premium price.

The proliferation of mega‑constellations (for example, broadband, Earth‑observation, IoT) has shifted the economics of space hardware. Unit‑mass BOMs that once justified the use of radiation‑hardened (rad‑hard) parts are now being re‑evaluated against high‑volume, potential low‑cost COTS alternatives. While the launch‑once, fly‑forever mindset still applies to high‑value GEO assets, LEO constellations demand rapid design cycles, aggressive price points, and the ability to iterate hardware generations. This white paper addresses the resulting tension between cost efficiency and mission assurance.

It compares the two approaches—COTS up screening versus directly sourcing space qualified components—through the lens of mission type taxonomy (new space LEO constellations, traditional MEO and GEO platforms, deep space probes, and hybrid legacy programs). The paper examines the technical attributes that make an integrated circuit space ready, outlines the practical considerations of a screening campaign, and quantifies the potential tradeoffs in cost, schedule, and total cost of ownership.

Key topics include:

  • Mission type guidance – How cost, reliability, and lifetime requirements differ among new space LEO constellations, traditional MEO and GEO satellites, deep space probes, and mixed heritage programs.
  • Critical screening parameters – Radiation hardness, thermal cycling endurance, outgassing, mechanical shock, and other hazard-specific tests, and how each maps to the hazard analyses defined for a given mission envelope.
  • Screening campaign economics – Typical test assets, lot size considerations, engineering effort, and the resulting cost per screened part versus the unit cost of a qualified part.
  • Risk mitigation strategies – Redundancy architectures, derating, spare parts pools, and in orbit health monitoring that allow designs based on COTS to meet reliability targets.
  • Advantages of space qualified parts – Full characterization for the harsh environment in space with the availability of the corresponding datasheet, heritage flight record, and reduced program level risk for missions where failure cost is prohibitive.
  • Lifecycle and total cost of ownership implications – How early component selection decisions affect constellation economics, yield and supply responsibility, upgrade pathways, and obsolescence management.

Readers of this document gain a practical decision framework that aligns component sourcing with a potential specific cost, risk, and schedule constraint of a specific mission class; enabling readers to make informed choices that balance economic efficiency with mission success in the current competitive space market.