STDA039 July 2026 F28377D-SEP , INA901-SP , SN54SLC8T245-SEP , TPS7A4501-SP , TPS7H1121-SEP , TPS7H1121-SP , TPS7H5020-SEP , TPS7H5020-SP , TPS7H6101-SEP
The space‑electronics design landscape is shaped by several critical environmental and material factors that must be addressed when selecting components for any mission, whether for a low‑cost LEO constellation or a long‑duration MEO, GEO, or deep‑space probe.
Radiation hardness is highly process‑dependent. Even devices fabricated on the same semiconductor node can display vastly different radiation responses because variations in circuit topology and the specific modules used affect susceptibility. In addition, many generalities about radiation tolerance are misleading. While a 65nm process is often considered immune to single‑event latch‑up (SEL), that immunity applies only to the low‑voltage (≅1.1V and below) circuits. If a product incorporates higher‑voltage blocks, those sections are more likely to be susceptible to SEL . Moreover, the presence of an epitaxial (epi) or silicon‑on‑insulator (SOI) substrate does not automatically guarantee SEL immunity for a CMOS device. For most CMOS products, an epi substrate has little effect on SEL susceptibility, and SOI provides SEL protection only when the field oxide (shallow trench isolation) extends completely through the active layer down to the buried oxide 1. Moreover, radiation hardness is not a standard control parameter in wafer fabs. Small changes in passivation thickness or stoichiometry between lots can cause dramatic shifts in total‑ionizing‑dose (TID) tolerance; one lot might survive 100krad (Si) while another from the same fab fails at just 10krad (Si). Consequently, radiation lot acceptance testing (RLAT) is essential for any part destined for space. Reliable qualification therefore demands a comprehensive testing regime that includes heavy‑ion testing for single‑event effects (SEE), displacement‑damage (DD) testing, and total ionizing dose (TID) testing to characterize cumulative dose performance.
Temperature extremes pose another major challenge. Spacecraft encounter wide temperature swings, requiring a design envelope of roughly –55°C to +125°C for robust operation. This range is far broader than the typical commercial (0°C to +70°C) or automotive Grade 3 (–40°C to +85°C) standards. Many COTS and automotive parts are only guaranteed within the limited commercial limits, so components must be assessed across the full temperature span for reliable performance in space.
Tin‑whisker risk arises from the pure‑tin (Sn) terminations that are common on many cost‑sensitive COTS and automotive devices (Figure 2-1). Under the thermal‑mechanical stresses of space, tin whiskers can grow, leading to short circuits between adjacent pins or to intermittent shorts when whiskers break off and contact other circuitry. Although conformal coatings provide some mitigation, these coatings do not eliminate the risk. Reliable space designs therefore avoid pure‑tin finishes and instead use Sn‑Pb alloy, nickel‑palladium‑gold (Ni‑Pd‑Au) plating, or similar terminations that suppress whisker formation.
Figure 2-1 Tin Whisker DevelopmentBond‑wire material considerations also influence reliability. Gold (Au) bond wires are preferred because these wires offer better performance under repeated thermal cycling due to the low temperature coefficient and resistance to corrosion of these wires. Copper (Cu) bond wires are increasingly used to reduce cost, but these wires require tighter process control. Cu wires have a higher temperature coefficient, making these wires more susceptible to neck‑break failures during rapid temperature cycles—a common condition in LEO. In harsh space environments, gold bond wires remain the preferred choice to minimize bond‑integrity failures.
Plastic outgassing and moisture absorption present further concerns. Package materials for plastic‑encapsulated parts are typically organic mold compounds that can both absorb moisture and outgas volatile organic species when exposed to vacuum and temperature extremes. The absorbed moisture lowers the dielectric strength of the package, which can lead to premature failures, while the outgassed contaminants can potentially condense on nearby components—especially optics, imaging sensors, and high‑impedance circuitry—degrading performance and reliability of the components.
Selecting packages made from low‑outgassing materials—those with total mass loss (TML) below 1% and collected volatile condensable material (CVCM) below 0.1%—and subjecting these packages to extended bake‑out and qualification testing mitigates these risks (1).
Taken together, these considerations form a comprehensive hazard‑analysis summary. Radiation hazards (TID, SEE, and DD) require parts that have been characterized for the specific process, validated through RLAT, and possibly supplemented with shielding or derating. Temperature extremes demand components rated to –55°C/+125°C and verification across the full range. Tin‑whisker concerns are addressed by avoiding pure‑Sn terminations in favor of alloyed or plated finishes. Bond‑wire reliability is maintained by selecting gold wires or, if copper is used, enforcing strict process controls and life testing is needed. Finally, outgassing and moisture issues are mitigated by choosing low TML and CVCM mold compounds and performing appropriate bake‑out and qualification procedures.
These generic considerations constitute the backbone of the space‑electronics design landscape and guide the selection of components—whether screened COTS or fully space‑qualified—across the entire spectrum of missions, from commercial LEO constellations to long‑duration MEO and GEO and deep‑space endeavors.