SWCU192 November 2021 CC1312R7 , CC1352P7 , CC2652P7 , CC2652R7
This example illustrates center-aligned PWM generation by channel 0 (see Figure 20-26). The waveform is synthesized on event output 0. The timer period is kept static, and the target value is set to half the period. Configure as follows:
Figure 20-26 Center-Aligned PWM
The duty-cycle of the generated PWM waveform is controlled by AUX_TIMER2:CH0PCC updates. Waveform generation on event output 0 continues until aborted by the user.