SWRA495L December 2015 – April 2025 CC1310 , CC1350 , CC2620 , CC2630 , CC2640 , CC2640R2F , CC2640R2F-Q1 , CC2642R-Q1 , CC2650 , CC2662R-Q1
The crystal frequency can be pulled by changing the load capacitance presented to the crystal. The parameter ΔF is the resonance frequency change of the crystal due to a change in the load capacitance on the board, whether this is internal or externally configured on the Launchpad. The pulling is given by Equation 6 around the specified (parallel) resonance frequency of the crystal.

CLMAX and CLMIN are the maximum and minimum load capacitance that can be presented to the crystal. These are different parameters from the CL specified on crystal data sheets. For more information, see CC13xx/CC26xx Hardware Configuration and PCB Design Considerations.