TIDUDI9A January 2018 – May 2025 ISOM8610
The mechanical switch is turned off. The common pullup resistor is 100 kΩ. Then, the broken wire detection is executed. Figure 3-3 shows a scope shot where channel 2 of the scope is connected to the control signal of the optical switch (BrWi) and channel 1 is connected to the OUT pin of one ISO121x (ChOut). Figure 3-4 shows a scope shot where channel 2 of the scope is connected to the input capacitor CIN of one ISO121x channel (V_cap) and channel 1 is connected to the OUT pin of one ISO121x (ChOut).
Figure 3-3 Group Broken Wire Detection,
Rpullup = 800kΩ/Channel - ChOut (2), BrWi (1)
Figure 3-4 Group Broken Wire Detection,
Rpullup = 800 kΩ/Channel - V_cap (2), BrWi (1) Figure 3-3 shows that as soon as the ground connection is enabled again, the ISO121x gives out a pulse. The device takes 24 ms until CIN is charged. Figure 3-4 shows that CIN is charged to a maximum value of 22.6 V. The 24 V is not reached because of the voltage drop across the pullup resistor, which equals to a current of 1.4 V / 100 kΩ = 14 µA.
Note that this current is not used by the ISO121x, but is leakage current caused by the different protection devices and leakage through the input capacitor. Also, the voltage drop across the pullup resistor is lower if the pullup resistor itself is lower. This result is also shown in the single-channel setup.
Figure 3-5 shows a zoom into Figure 3-4.
Figure 3-5 Zoom Into (Figue 3-4: Group
Broken Wire Detection, Rpullup = 800 kΩ/Channel - V_cap (2), BrWi
(1)) - V_cap (1), ChOut (2)After the ISO1211 is enabled again, CIN is discharged and the ISO1211 starts operating. It takes around 14 µs until first, there is a solid GND connection for the ISO1211 established, and second, enough current (2.2 mA, typical, taken from ISO121x data sheet) is flowing through RSENSE while at the same time the voltage at the SENSE pin is still above the logic high level, so above 13.65 V - 1.2 V (hysteresis) = 12.45 V. Now, the output of the ISO1211 switches high. As soon as the energy stored in CIN is not anymore high enough to supply 2.2 mA and keep the voltage at the SENSE pin in the high level range, the output of the ISO1211 switches low.
For this configuration, the resulting pulse lasts around 50.5 µs.