TIDUDI9A January 2018 – May 2025 ISOM8610
The broken wire detection works as expected. However, several observations need to be considered when implementing the broken wire detection.
The higher the pullup resistor to 24 V, the lower the maximum voltage at CIN. Also, consider the leakage current through protection elements and the capacitor. For example:
In general, it is important to choose an opto-emulator switch that turns on and off quickly. If the opto-emulator switch turns on too slow, CIN will already be discharged too much before the ISO121x has a solid GND connection. Then, no output pulse is created.