TIDUEV2 October 2025
The sample rate of the USB input is determined by the sample rate settings for the audio device in the settings of the PC. Access the device properties to set the sample rate. Figure 3-5 shows the use of 24-bit, 190000Hz for testing. Microsoft® Windows® requires restarting any software that plays an audio source after changing the rate.
Figure 3-5 Speaker Properties Menu for Selecting Sample Rate