JAJSP34G October 2011 – September 2022 TPS40422
PRODUCTION DATA
The pu bit sets the default to either operate any time power is present or for the on/off to be controlled by CNTLx pins and PMBus OPERATION command. This bit is used in conjunction with the 'cp', 'cmd', and 'on' bits to determine start up.
Bit Value | ACTION |
---|---|
0 | Channel powers up any time power is present regardless of state of the CNTLx pins. |
1 | Channel does not power up until commanded by the CNTLx pins and OPERATION command as programmed in bits [2:0] of the ON_OFF_CONFIG register. |