TIDUF36A May 2023 – December 2023 DRV8328
Figure 4-9 through Figure 4-12 show the motor winding current and winding voltage waveforms at a 18-V DC input and a 10-ARMS, 33-A winding current, and the thermal images under the same conditions. The testing is done at 15% duty cycle.
Current waveform and thermal behavior when a large current is passed through the device can be observed. The input power is 18 V at 4 A to 5.5 A, 72 W to 100 W.
Under the provided test conditions, in the case of 10-ARMS current, the current of the maximum MOSFET is 49.3°C.
Under the given test conditions, in the case of 33-ARMS current, the current of the maximum MOSFET is 97.1°C.
Figure 4-13 shows load test setup with a dynamometer.