SLUSE99C September 2021 – January 2023 BQ25180
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
When battery voltage is above the VBATSC but lower than VLOWV threshold, the battery is charged with the precharge current level. The precharge current (IPRECHARGE) can be programmed through I2C and can be adjusted by the host. Once the battery voltage reaches VLOWV, the charger will then operate in Fast Charge mode, charging the battery at ICHG.
During precharge, the safety timer is set to 25% of the safety timer value during fast charge. In the case where termination is disabled, precharge current is set to 20% of fast charge current setting.