SLLSG06 December 2024 MCF8315D
PRODUCTION DATA
Align braking is used to stop the motor at a user configured angle when a brake command is received either through a logic High signal on the BRAKE pin or by setting BRAKE_INPUT to 01b. In this mode, on receiving the brake command, MCF8315D reduces the motor speed to a value defined by BRAKE_SPEED_THRSHOLD before bringing the motor to an "aligned stop" by continuously injecting a DC current through a particular phase pattern. The phase pattern during align brake is generated based on the angle at which align needs to be performed - this angle can be configured either as the last commutation angle when BRAKE_SPEED_THRESHOLD is reached (ALIGN_BRAKE_ANGLE_SEL = 0b) or set directly using ALIGN_ANGLE (when ALIGN_BRAKE_ANGLE_SEL = 1b). The current limit during align braking is configured through ALIGN_OR_SLOW_CURRENT_ILIMIT.