Before beginning a design using the device,
consider the following:
- Make VIN, PGND, and SW traces as wide as possible
to reduce trace impedance and improve heat dissipation.
- Place the power components (including input and
output capacitors, the inductor, and the IC) on the top side of the PCB. To shield and
isolate the small signal traces from noisy power lines, insert at least one solid ground
inner plane.
- Placement of the VIN decoupling capacitors are
important for the power MOSFET robustness. A 1μF/25V/0402 ceramic high-frequency bypass
capacitor on each VIN pin (pins 4 and 12) is required, connected to the adjacent PGND
pins (pins 5 and 11 respectively). Place the remaining ceramic input capacitance next to
these high frequency bypass capacitors. The remaining input capacitance can be placed on
the other side of the board, but use as many vias as possible to minimize impedance
between the capacitors and the pins of the IC.
- Place as many vias as possible below and near the
PGND pins. This action minimizes parasitic impedance and also lowers thermal
resistance.
- Use vias
near both VIN pins and provide a low impedance connection between them through an
internal layer. A via can also be placed below each of the VIN pins.
- Place the VCC decoupling capacitor as close as
possible to the device, with a short return to PGND (pin 5). Make sure the VCC
decoupling loop is small and use traces with a width of 12 mil or wider to route the
connection.
- Place the BOOT capacitor as close as possible to
the BOOT and SW pins. Use traces with a width of 12 mil or wider to route the
connection.
- The PCB trace, which connects
the SW pin and high-voltage side of the inductor, is defined as switch node.
The switch node must be as short and wide as possible.
- If using external feedback, always place the
feedback resistors near the device to minimize the FB trace distance, no matter
single-end sensing or remote sensing.
- For remote sensing, the connections
from the FB voltage divider resistors to the remote location must be a differential
pair of PCB traces, and must implement Kelvin sensing across a bypass capacitor of
0.1μF or higher. The ground connection of the remote sensing signal must be
connected to GOS pin. The VOUT connection of the remote sensing signal
must be connected to the feedback resistor divider with the bottom feedback resistor
terminated to the GOS pin. To maintain stable output voltage and minimize the
ripple, the pair of remote sensing lines must stay away from any noise sources such
as inductor and SW nodes, or high frequency clock lines. TI recommends to shield the
pair of remote sensing lines with ground planes above and below.
- For single-end sensing, connect the
top feedback resistor between the FB pin and the output voltage to a high-frequency
local output bypass capacitor of 0.1μF or higher, and short GOS to AGND with a short
trace.
- Connect the AGND pin (pin 19) to the PGND pins
(pins 5 and 11) beneath the device.
- Avoid routing the PG signal and any other noisy
signals in the application near noise sensitive signals, such as VOS/FB and GOS to limit
coupling.
- See Layout Example for the layout recommendation.