JAJU732C June 2019 – July 2022
During the transition from interval one to two, there exists a small dead time where the inductor-stored energy discharges the output capacitances of the MOSFETs and holds them close to zero voltage before they are turned on. This phenomenon, where the voltage across the MOSFET is close to zero at turn on, is referred to as zero voltage switching (ZVS). This is a major advantage with this topology, where due to the natural lagging current in one of the bridges, the inductive stored energy causes ZVS of all of the lagging bridge switches and some of the switches of the leading bridge. This depends on the stored inductive energy (EL = 0.5LI2) available to charge and discharge the output capacitances of MOSFETs (EC = 0.5CV2).
When transition happens from interval one to two, the primary side switches Q1 and Q5 continue conduction, whereas in the secondary, Q6 and Q7 turn off and Q5 and Q8 turn on. Initially the voltage across Q6 and Q7 is zero when they are conducting, and Q5 and Q8 block the entire secondary voltage. During dead time, when all of the switches in the secondary are off, the inductor-stored energy circulates current which discharges the capacitor across MOSFETs Q5 and Q8 to zero and charges the capacitor across MOSFETs Q6 and Q7 to the full secondary voltage. The current commutation is shown in Figure 2-11.
Once the capacitors have been charged and discharged, the current must continue to flow. The current will flow through the diodes D5 and D8, thereby clamping the voltage across MOSFETs Q5 and Q8 to zero as shown in Figure 2-12. During the next interval, MOSFETs Q5 and Q8 are turned on at zero voltage, thereby reducing turn on losses completely. The arrow close to the diode indicates that the diode is conducting and the MOSFET is off.
Similarly, zero voltage switching across the switches of the primary during the transition from interval 2 to 3 is explained in the following section. When transition happens from interval two to three, the secondary side switches Q5 and Q8 continue conduction, whereas in the primary, Q1 and Q4 turn off and Q2 and Q3 turn on. Initially, the voltage across Q1 and Q4 is zero when they are conducting, and Q2 and Q3 block the entire secondary voltage. During dead time when all of the switches in the primary are off, the inductor stored energy circulates current, which discharges the capacitor across MOSFETs Q2 and Q3 to zero and charges the capacitor across MOSFETs Q1 and Q4 to the full primary voltage. The current commutation is shown in Figure 2-13.
Once the capacitors have been charged and discharged, the current must continue to flow. The current will flow through diodes D2 and D3, thereby clamping the voltage across MOSFETs Q2 and Q3 to zero as shown in Figure 2-14. During the next interval, MOSFETs Q2 and Q3 are turned on at zero voltage, thereby reducing turn on losses completely. The arrow close to the diode indicates that the diode is conducting and the MOSFET is off.