SPRABJ8B September 2022 – November 2023 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P4
The AM263x and AM263Px one-time programmable, e-Fuse memory can be utilized for storing customer cryptographic keys and other information specific to individual devices. These e-Fuse memory locations can only be programmed when the target device VPP, e-Fuse power pin, is powered by a 1.7 V nominal output voltage, 100 mA peak current supply. This 1.7V VPP power supply can be onboard or off-board. The specific placement of the VPP supply and implementation depend on how the e-Fuse memory will be utilized by the designer. The implementation should follow the diagram shown in Figure 2-18
The AM263Px has the option to source VPP internally using the ANALDO. The ANALDO must be overwritten to provide 1.7V during e-Fuse programming, then reverted back to normal operation.
The e-Fuse programming typically follows one or both of the following scenarios:
If the factory programming scenario is all that is required for a product, then it is typically preferable for the VPP power supply to be implemented off-board since this reduces the number of supplies required to be placed on the PCB assembly. The VPP supply would only be used during this programming sequence, so keeping it on the board would not be an efficient use of PCB floor plan area, BOM cost or test time.
However, if the e-Fuse memory must be programmed outside the factory environment, the VPP power must either be supplied from an onboard component or from an attached accessory board that can supply this power as needed.
In the case of the TMDSCNCD263 controlCard evaluation module design, the VPP supply was left on the board to enable convenient e-fuse programming by customers experimenting with this process. On the controlCard the TLV75801PDRVR LDO, U66, was used to drop down the 3.3 V system I/O voltage to the VPP 1.7 V. Additionally, the GPIO expander, U50 was used to toggle the VPP_LDO_EN pin to enable/disable the LDO in the required sequence for e-Fuse programming.
For the full VPP electrical requirements and e-Fuse programming sequence, see the VPP Specifications for One-Time Programmable (OTP) eFuses section in the AM263x Sitara™ Microcontroller Data Sheet or AM263Px Sitara™ Microcontroller Data Sheet.