UniFlash
is a software tool for programming onboard flash on TI mmWave sensors. UniFlash
provides both graphical and command-line interfaces. The UniFlash tool can be used
to program the flash with the final app image.
TI Reference
Collaterals
Note: TI supports multiple
interfaces for flashing the onboard memory on a EVM. Interfaces like UART, JTAG,
Ethernet and CAN are supported and TI also provides the tools to support the
flashing. The path below in the SDK provides all the details and TI recommends to go
through the contents to understand all the flashing utilities available form TI. The
file path is provided with reference to AWR2944 device. Users can select the folder
corresponding to the device as well. The tools usage remain the same.
ti/mmwave_mcuplus_sdk_xx_xx_xx_xx/mcu_plus_sdk_awr294x_xx_xx_xx_xx/docs/api_guide_awr294x/TOOLS_FLASH.html