SPRUIU1D July 2020 – December 2024 DRA821U , DRA821U-Q1
A UTC accepts Transfer Request records from the UDMA-C and performs a sequence of transactions as specified in the TR record in accordance with the address generation algorithm that is specified in the Transfer Request format specification. The UTC will wait until an optional triggering event has occurred to load the channel state into one of its read or write engines so that the data movement operations can be completed. The UTC will complete the specified transactions until it either has transferred a pre-set number of bytes or until it has reached a point in the sequence where the TR indicates that a trigger is required to continue execution. When either of these two conditions is met, the UTC will save off the current state of the channel and will wait until the channel is re-triggered at which point the TR execution will continue. Once the entire Transfer Request specified sequence of data transfers has completed, the UTC will wait to ensure that all outstanding writes have landed at their respective destination endpoints and will then return a Transfer Response message back to the UDMA-C indicating the success or failure of the Transfer Request. The UTC processes Transfer Request operations on a given channel with strong ordering such that all Transfer Response operations will be returned in an order corresponding to the exact order that Transfer Request operations were issued.