SPRUIU1D July 2020 – December 2024 DRA821U , DRA821U-Q1
The Element Type field allows the user to specify the basic unit that is used for the innermost loop. If the FMTFLAGS field is not present then the UTC will assume a value of 0 which is a byte size element. The element type also allows for the some expansion or contraction of the element size from the source to the destination.
| Encoding | Definition |
|---|---|
| 0 | 1 Byte per element |
| 1 | 1.5 Bytes(12 bits) per element |
| 2 | 2 Bytes per element |
| 3 | 3 Bytes per element |
| 4 | 4 Bytes per element |
| 5 | 8 Bytes per element |
| 6 | 16 Bytes per element |
| 7 | 32 Bytes per Element |
| 8 | 1 Byte per Input Element 2 Bytes per Output Element |
| 9 | 1.5 Bytes per Input Element 2 Bytes per Output Element |
| 10 | 2 Bytes per Input Element 1 Byte per Output Element |
| 11 | 2 Bytes per Input Element 1.5 Bytes per Output Element |
| 12-15 | Reserved for Future Use |