SPRUIU1D July 2020 – December 2024 DRA821U , DRA821U-Q1
The Timeout Error Info Register contains information about the number of Timeout errors that have occurred.
| Bits | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31:2 | Reserved | r | 0x0 | Reserved. Read as 0. |
| 1:0 | timeouts | r/wtd | 0x0 |
This field contains information about how many transactions have timed out since the last one was serviced. Writing to this register decrements the contents by the value written. For instance, if the value is 2 and a 1 is written, the value will decrement to 1. If this field is non-0 when the interrupt is cleared by writing to the Error Interrupt Enabled Status/Clear Register (Base Address + 0x24) the interrupt will be re-issued. The value saturates at 3, so if there are more than three pending it will be unknown exactly how many have occurred. If the value is saturated at 3 and a value of 3 is written, the value will turn to 0. Read 0 – No pending timeout interrupts 1 – One pending timeout interrupt 2 – Two pending timeout interrupts 3 – Three or more pending timeout interrupts |