STDA017 November   2025 TPS7A33 , TPS7A4501-SP , TPS7A47 , TPS7A47-Q1 , TPS7A4701-EP , TPS7A52 , TPS7A52-Q1 , TPS7A53 , TPS7A53-Q1 , TPS7A53A-Q1 , TPS7A53B , TPS7A54 , TPS7A54-Q1 , TPS7A57 , TPS7A8300 , TPS7A83A , TPS7A84 , TPS7A84A , TPS7A85A , TPS7A90 , TPS7A91 , TPS7A92 , TPS7A94 , TPS7A96 , TPS7B7702-Q1 , TPS7H1111-SEP , TPS7H1111-SP

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction to Parallel LDOs Using Ballast Resistors
  5. 2Noise Analysis of Parallel LDOs Using Ballast Resistors
  6. 3LDO Output Impedance
  7. 4Strategies on Reducing the Noise of the Parallel LDO System
  8. 5Noise of Parallel LDOs Using Ballast Resistors
    1. 5.1 TPS7A57
    2. 5.2 TPS7A94
  9. 6Noise Measurements of Alternative Parallel LDO Architectures
    1. 6.1 TPS7B7702-Q1
  10. 7Conclusion
  11. 8References

Noise Analysis of Parallel LDOs Using Ballast Resistors

As described in reference [1], parallel LDOs using ballast resistors can be redrawn as shown in the schematic in Figure 2-1, and the VLOAD formula is provided in equation 1.

TPS7A94 TPS7A96 TPS7A57 TPS7B7702-Q1 Equivalent Model for n Parallel LDOs Using
                    Ballast ResistorsFigure 2-1 Equivalent Model for n Parallel LDOs Using Ballast Resistors
Equation 1. VLOAD=n=1nVOUTn+VEnRBn - ILOADn=1n1RBn

Assume a parallel network in which no LDO regulates another LDO, and each feedback loop of the regulator operates independently of the others. Let ZOUTn denote the output impedance of the nth LDO in the parallel array. Since the noise analysis is performed under steady‑state conditions, the load current ILOAD contains no AC component; consequently, the load current is constant (for example, the frequency content is zero). Equation 1 can therefore be simplified by applying these assumptions.

  1. Set RBn = ZOUTn + RB = "R"
  2. Replace VOUT1, VOUT2,…, VOUTn with noise source en
  3. Set VE1 = VE2 = … = VEn = 0V
  4. Set ILOAD = 0

Using these assumptions, rewrite equation 1 as equations 2 and 3.

Equation 2. en, LOAD=n=1nenR n=1n1R=n=1nenRnR=n=1nenn=n=1nenn2
Equation 3. e n ,   L O A D = e n n

The output noise of the parallel LDOs is reduced by the square root of the number of LDOs in parallel. Fundamentally, these assumptions imply that all paralleled LDOs exhibit identical intrinsic noise (because the same LDO IC is used), operate at the same temperature, generate zero or negligible error‑voltage, use the same ballast resistors with low tolerance (< 1%), and are closely matched in output impedance (ZOUT).