SWRA726 March 2022 CC1120 , CC1121 , CC1201 , CC1310 , CC1311P3 , CC1311R3 , CC1312PSIP , CC1312R , CC1312R7 , CC1314R10 , CC1350 , CC1352P , CC1352R , CC1354P10 , CC1354R10 , CC2340R5-Q1 , CC2640R2L , CC2651R3 , CC2652P , CC2652P7 , CC2652R , CC2652R7 , CC2652RB , CC2652RSIP , CC3130 , CC3135MOD , CC3230S , CC3235MODAS , CC3235MODASF , CC3235MODSF , CC3235S , WL1801MOD , WL1805MOD , WL1807MOD , WL1831 , WL1831MOD , WL1835MOD , WL1837MOD
Calibration method described below can’t be high precise as it’s impossible to make a precision short, open and matched loads on the board, especially for frequencies above 2 GHz due to parasitic elements (short load will always have an inductance and open load a fringing capacitance), but reasonably sufficient for antenna in-device measurement and matching.
An example of typical Pi-matching network (not in scale) and DC blocking capacitor on PCB are shown on Figure 4-15.
Figure 4-15 Typical Matching NetworkMatching components should be removed (if not already) from the board and matching network isolated from a transceiver (for example, removed DC blocking capacitor). An example with connected semi-rigid cable and SOL calibration point is shown on Figure 4-16.
Figure 4-16 Example of Semi-Rigid Coaxial Cable Connection to Matching Network
Figure 4-17 VNA Calibration for
Open Load
Figure 4-18 VNA Calibration for
Short Load
Figure 4-19 VNA Calibration for
Matched 50-Ohm LoadDepending on what VNA model users use, an option for delay can have different menu name (for example, port extension). Port extension allows users to move electrically a measurement reference plane after the calibration.
Figure 4-20 shows uncompensated delay after the calibration with short load connected at 868 MHz frequency. So, the VNA is showing connected short load as not the short load. If the compensation will not be done, it can compromise measured impedance value of the antenna, so the final matching of the antenna will be incorrect and far in comparison with a real antenna’s behavior.
Figure 4-20 Uncompensated Delay with
Short-Load ConnectedAfter the compensation, the marker should indicate the Short load. Compensated delay of 32.82 ps is shown on Figure 4-21.
Figure 4-21 Compensated Delay with
Short-Load ConnectedCompensation (port extension) can be done with open load as well. The short load just better as gives higher level of reflections to VNA port. In reality, short and open loads have slightly different delays even for the precision calibration kits.
It is good practice to measure losses (skin effect losses) and compensate them if VNA supports this feature.