SBAA535A March   2022  – March 2024 ADC128D818 , ADS1000 , ADS1000-Q1 , ADS1013 , ADS1013-Q1 , ADS1014 , ADS1014-Q1 , ADS1015 , ADS1015-Q1 , ADS1018 , ADS1018-Q1 , ADS1100 , ADS1110 , ADS1112 , ADS1113 , ADS1113-Q1 , ADS1114 , ADS1114-Q1 , ADS1115 , ADS1115-Q1 , ADS1118 , ADS1118-Q1 , ADS1119 , ADS1120 , ADS1120-Q1 , ADS112C04 , ADS112U04 , ADS1130 , ADS1131 , ADS1146 , ADS1147 , ADS1148 , ADS1148-Q1 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1158 , ADS1216 , ADS1217 , ADS1218 , ADS1219 , ADS1220 , ADS122C04 , ADS122U04 , ADS1230 , ADS1231 , ADS1232 , ADS1234 , ADS1235 , ADS1235-Q1 , ADS1243-HT , ADS1246 , ADS1247 , ADS1248 , ADS124S06 , ADS124S08 , ADS1250 , ADS1251 , ADS1252 , ADS1253 , ADS1254 , ADS1255 , ADS1256 , ADS1257 , ADS1258 , ADS1258-EP , ADS1259 , ADS1259-Q1 , ADS125H01 , ADS125H02 , ADS1260 , ADS1260-Q1 , ADS1261 , ADS1261-Q1 , ADS1262 , ADS1263 , ADS127L01 , ADS1281 , ADS1282 , ADS1282-SP , ADS1283 , ADS1284 , ADS1287 , ADS1291 , LMP90080-Q1 , LMP90100 , TLA2021 , TLA2022 , TLA2024

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Introduction
  5. Data Sheet Timing and Nomenclature
  6. What Causes Conversion Latency in a Delta-Sigma ADC?
  7. Digital Filter Operation and Behavior
    1.     8
    2.     9
    3. 4.1 Unsettled Data Due to an ADC Operation
  8. ADC Features and Modes that Affect Conversion Latency
    1. 5.1 First Conversion Versus Second and Subsequent Conversion Latency
    2. 5.2 Conversion Mode
    3. 5.3 Programmable Delay
    4. 5.4 ADC Overhead Time
    5. 5.5 Clock Frequency
    6. 5.6 Chopping
  9. Analog Settling
  10. Important Takeaways
  11. Cycle Time Calculation Examples
    1. 8.1 Example #1: Using the ADS124S08
    2. 8.2 Example #2: Changing the Conversion Mode
    3. 8.3 Example #3: Changing the Filter Type
    4. 8.4 Example #4: Changing the Clock Frequency
    5. 8.5 Example #5: Enabling Chop and Reducing the Number of Conversions per Channel
    6. 8.6 Example #6: Scanning Two Channels With Different System Parameters
    7. 8.7 Example #7: Using the ADS1261
    8. 8.8 Example #8: Changing Multiple Parameters Using the ADS1261
  12. Summary
  13. 10Revision History

Conversion Mode

Closely related to first-conversion versus second-and-subsequent conversion latency is how conversions are triggered by the user. Many ADCs offer multiple modes to trigger a conversion. Examples of these modes include continuous-conversion, single-shot, or pulse-convert. Table 5-2 shows the available conversion modes in the ADS124S08.

Table 5-2 Conversion Mode Selection in the ADS124S08 Data Rate (DATARATE) Register

BIT

FIELDTYPERESETDESCRIPTION

5

MODE

R/W

0h

Conversion mode selection

Configures the ADC for either continuous-conversion or single-shot mode.

0 : Continuous-conversion mode (default)

1 : Single-shot conversion mode

Continuous-conversion mode automatically starts a new conversion immediately after the previous conversion period completes. This process continues indefinitely until stopped by the user. Assuming a settled analog input, the ADC outputs settled data after each conversion period for second and subsequent conversions. This process is shown in Figure 5-2.

Conversely, single-shot mode produces one conversion result and then waits for user input before restarting the conversion process. When the user requests a new conversion in single-shot mode, the ADC resets the digital filter each time. Therefore, single-shot conversions are always affected by the first-conversion latency that was previously described in Section 5.1. This is true even if the same channel is repeatedly sampled without any ADC operations or step inputs.

The difference between conversion modes may also be included in the conversion latency table. For example, Table 5-1 indicates that first conversion latency applies to both continuous- and single-shot conversion mode for the ADS124S08, while second and subsequent conversion latency only applies to continuous-conversion mode. Refer to the specific ADC data sheet to identify available conversion modes as well as how each mode affects the overall conversion latency.