SBAA535A March 2022 – March 2024 ADC128D818 , ADS1000 , ADS1000-Q1 , ADS1013 , ADS1013-Q1 , ADS1014 , ADS1014-Q1 , ADS1015 , ADS1015-Q1 , ADS1018 , ADS1018-Q1 , ADS1100 , ADS1110 , ADS1112 , ADS1113 , ADS1113-Q1 , ADS1114 , ADS1114-Q1 , ADS1115 , ADS1115-Q1 , ADS1118 , ADS1118-Q1 , ADS1119 , ADS1120 , ADS1120-Q1 , ADS112C04 , ADS112U04 , ADS1130 , ADS1131 , ADS1146 , ADS1147 , ADS1148 , ADS1148-Q1 , ADS114S06 , ADS114S06B , ADS114S08 , ADS114S08B , ADS1158 , ADS1216 , ADS1217 , ADS1218 , ADS1219 , ADS1220 , ADS122C04 , ADS122U04 , ADS1230 , ADS1231 , ADS1232 , ADS1234 , ADS1235 , ADS1235-Q1 , ADS1243-HT , ADS1246 , ADS1247 , ADS1248 , ADS124S06 , ADS124S08 , ADS1250 , ADS1251 , ADS1252 , ADS1253 , ADS1254 , ADS1255 , ADS1256 , ADS1257 , ADS1258 , ADS1258-EP , ADS1259 , ADS1259-Q1 , ADS125H01 , ADS125H02 , ADS1260 , ADS1260-Q1 , ADS1261 , ADS1261-Q1 , ADS1262 , ADS1263 , ADS127L01 , ADS1281 , ADS1282 , ADS1282-SP , ADS1283 , ADS1284 , ADS1287 , ADS1291 , LMP90080-Q1 , LMP90100 , TLA2021 , TLA2022 , TLA2024
Table 8-8 reports the system parameters that determine the cycle time in Example #3:
| PARAMETER | VALUE |
|---|---|
| ADC | ADS124S08 |
| ODR | 1000 SPS |
| Filter type | Low-latency |
| Clock frequency | 4.096 MHz (default) |
| Conversion mode | Single-shot |
| Programmable delay | 14 ∙ tMOD (default) |
| Chopping | Disabled |
| Conversions per channel | 3 |
| # of channels | 2 |
Example #3 keeps all of the same system parameters as Example #2 with the exception of switching to the ADS124S08 low-latency filter. This choice reduces the conversion latency for each first conversion.
While not shown in this document, the ADS124S08 data sheet identifies the first-conversion latency, tFC, using the low-latency filter at ODR = 1000 SPS as 1.156 ms. This time assumes that the default clock frequency, fCLK, of 4.096 MHz is used, which is the case for this example. Also, this time includes the ADC overhead but does not include the programmable delay, tDELAY. Equation 14 calculates the value of tDELAY in microseconds using the default value of tDELAY = 14 ∙ tMOD and fCLK = 4.096 MHz:
The ADS124S08 programmable delay applies to each conversion using single-shot mode, resulting in a first conversion latency including programmable delay, tFC_TOTAL, as per Equation 15:
Finally, there is no need to consider additional latency due to chopping. Since all three conversions use single-shot mode and therefore are subject to tFC_NEW, the scan time for one channel, tCH, is given by Equation 16. This assumes that the user starts the next conversion on each channel immediately after the previous conversion result is ready:
Equation 17 calculates the cycle time, tCYCLE, using the result from Equation 16:
Ultimately, the cycle time for this example is 7.266 ms for 6 conversion results. Figure 8-3 depicts a timing diagram for the example system given the design parameters.