SBAA677 March 2025 ADC08DJ3200 , ADC08DJ5200RF , ADC09DJ1300 , ADC09DJ800 , ADC09QJ1300 , ADC09QJ800 , ADC09SJ1300 , ADC09SJ800 , ADC12DJ1600 , ADC12DJ2700 , ADC12DJ3200 , ADC12DJ4000RF , ADC12DJ5200RF , ADC12DJ800 , ADC12QJ1600 , ADC12QJ800 , ADC12SJ1600 , ADC12SJ800 , ADC32RF52 , ADC32RF54 , ADC32RF55 , ADC32RF72 , ADC34RF52 , ADC34RF55 , ADC34RF72 , ADC3548 , ADC3549 , ADC3568 , ADC3569 , ADC3643 , ADC3648 , ADC3649 , ADC3660 , ADC3668 , ADC3669
Following are five active (amplifier) or passive (balun) analog input network metrics that can help keep the input network design focused and on track:
These metrics encapsulate the entire front-end interface design, not just the analog-to-digital converter (ADC). Considering these metrics first can help decide between an active or passive front end.
The following section shows five different front-end designs to compare these metric trade-offs, as shown in Figure 2-1.
Figure 2-1 Five Front-end Designs: Balun Only, an LNA, a Balun Plus an FDA, a Single-Ended FDA and the TRF1208