SBASAW5 December 2025 ADS112C14 , ADS122C14
PRODUCTION DATA
GPIO3 can be configured as a dedicated DRDY output pin (GPIO3_CFG[1:0] = 10b or 11b, GPIO3_SRC = 1b). DRDY drives high when conversions are started, and drives low when conversion data are ready, as shown in Figure 7-27. DRDY drives back high after the eighth bit of the MSB conversion data is transmitted, as shown in Figure 7-25.
If a new conversion completes in the middle of or after the RDATA command byte, the state of the DRDY pin at the end of the data read operation signals whether the old or the new result is output. If the old result is output, DRDY stays low, indicating that the new result is not read out, as shown in Figure 7-26. The new conversion result is output when DRDY is high at the end of the data read operation.
If conversion data are not read, DRDY pulses high tW(DRH) before the next falling edge, as shown in Figure 7-27.
Whenever the device is programmed to enter standby mode (STBY_MODE bit = 1b) after conversions stopped, DRDY is driven back high 4 tMOD after transitioning low. Figure 7-28 shows an example of the DRDY pin behavior when entering standby mode using single-shot conversion mode.
Polling the DRDY bit or the state of the DRDY pin to check for the completion of the conversion is not practical in this particular scenario (STBY_MODE bit = 1b) because of the short period the DRDY pin is low. Use one of the other available options to determine when new data are available, such as the DRDY pin falling edge, reading the conversion counter, or waiting a fixed amount of time equal to or longer than the conversion period.