SBASAW5 December 2025 ADS112C14 , ADS122C14
PRODUCTION DATA
The RDATA command loads the output shift register with the most recent conversion result. Reading conversion data must be performed as shown in Figure 7-17 and Figure 7-18 by using two I2C communication frames. The first frame is an I2C write operation where the R/W bit at the end of the address byte is 0b to indicate a write. In this frame, the controller sends the RDATA command to the ADS1x2C14. The second frame is an I2C read operation where the R/W bit at the end of the address byte is 1b to indicate a read. The ADS1x2C14 reports the latest ADC conversion data in this second I2C frame. If a conversion finishes in the middle of the RDATA command byte, the state of the DRDY pin at the end of the data read operation signals whether the old or the new result is loaded. If the old result is loaded, DRDY stays low, indicating that the new result is not read out. The new conversion result loads when DRDY is high at the end of the data read transaction.
Figure 7-19 shows an example of reading conversion data from a 24-bit device with the STATUS header and CRC enabled (STATUS_EN = 1b, I2C_CRC_EN = 1b). The CRC covers the 16-bit STATUS header and the 24-bit conversion data.
The device outputs a zero-padding byte between the conversion data and CRC byte as shown in Figure 7-20, when the CRC is enabled for the 16-bit device. The zero-padding byte is included in the CRC calculation.