SBOSAJ7A October 2025 – December 2025 TMP4719
PRODUCTION DATA
The TMP4719 T_CRIT pin is an active-low, open-drain output which is asserted at the end of a conversion cycle when the measured temperature exceeds a T_CRIT Limit defined in the T_CRIT limit registers. A T_CRIT Status Register flag is set at the end of a conversion cycle when the measured temperature exceeds a T_CRIT Limit. The T_CRIT pin deasserts at the end of a conversion cycle if the temperature measurement is less than the T_CRIT limit – T_CRIT Hysteresis. The T_CRIT Hysteresis is set in the Hysteresis register.
When the TMP4719 is set in interrupt mode, the status register flag is cleared by reading the status register. The Status Register flag continues to set after the end of a conversion cycle until the temperature measurement is below the T_CRIT limit – T_CRIT Hysteresis value or the device is reset. T_CRIT has no mask bit. Note that reading the Status Register sets the ALERT mask bit of the Configuration Register if any flag in the Status Register, except the ADC_Busy flag and Remote Diode Fault flag, is set. The ALERT mask bit does not mask the T_CRIT pin, which means the clearance of ALERT mask bit has no influence on T_CRIT pin, and T_CRIT has no mask bit. There are separate T_CRIT Limit values and status register flags for the remote and local temperature measurements.
Figure 7-7 shows the behavior of the T_CRIT pin and flags in interrupt mode.
When the TMP4719 is in comparator mode, the status register flag is only cleared at the end of a conversion cycle if the temperature measurement is below the T_CRIT limit – T_CRIT Hysteresis value. Figure 7-8 shows the behavior of the T_CRIT pin and flags in comparator mode.