SLAAED9 November 2023 TAA5412-Q1 , TAC5311-Q1 , TAC5312-Q1 , TAC5411-Q1 , TAC5412-Q1
This register is the live Interrupt status register for channel 1 fault diagnostic
| Bit | Field | Type(1) | Reset | Description |
|---|---|---|---|---|
| 7 | IN_CH1_LIVE | R | 0b | Input Channel-1 Open Inputs
0b = No Open Inputs 1b = Open Inputs |
| 6 | IN_CH1_LIVE | R | 0b | Input Channel-1 Inputs
Shorted 0b = No Input Shorted 1b = Input Shorted to each other |
| 5 | IN_CH1_LIVE | R | 0b | Input Channel-1 INP Shorted
to GND 0b = INP not shorted to GND 1b = INP shorted to GND |
| 4 | IN_CH1_LIVE | R | 0b | Input Channel-1 INM Shorted
to GND 0b = INM not shorted to GND 1b = INM shorted to GND |
| 3 | IN_CH1_LIVE | R | 0b | Input Channel-1 INP Shorted
to MICBIAS 0b = INP not shorted to MICBIAS 1b = INP shorted to MICBIAS |
| 2 | IN_CH1_LIVE | R | 0b | Input Channel-1 INM Shorted
to MICBIAS 0b = INM not shorted to MICBIAS 1b = INM shorted to MICBIAS |
| 1 | IN_CH1_LIVE | R | 0b | Input Channel-1 INP Shorted
to VBAT_IN 0b = INP not shorted to VBAT_IN 1b = INP shorted to VBAT_IN |
| 0 | IN_CH1_LIVE | R | 0b | Input Channel-1 INM Shorted
to VBAT_IN 0b = INM not shorted to VBAT_IN 1b = INM shorted to VBAT_IN |
In addition to the channel registers, there are also interrupt registers that contain various faults. The first of these registers, INT_LIVE0 (P1_R60), contains the boost-protection fault flags as well as the ASI bus clock error and PLL lock status. The PLL lock status is not a fault, but provides a method to monitor when the state of the PLL changes. For more information on ASI bus clock errors, see the device data sheet.