Figure 2-6 shows what parameters are included in Interrupts block.
The MCAN module contains one event
publisher (CPU_INT) that manages MCAN interrupt requests (IRQs) to the CPU subsystem
by a static event route. Figure 2-11 shows the integration of the MCAN module in the device.
- MCAN Interrupts
- Enable MCAN Interrupts:
the MCAN core has two interrupt lines and 30 internal interrupt sources.
Each source can be configured to drive one of the two interrupt lines.
The MCAN core provides two interrupt requests Interrupt Line0 and
Interrupt Line1.
- Enable MCAN Line
Interrupts: defines which interrupt lines are used in the application.
- Interrupts To Trigger In
Line0: defines which interrupt sources are assigned to Interrupt Line0.
- Interrupts To Trigger In
Line1: defines which interrupt sources are assigned to Interrupt Line1.
- MSPM0 Interrupts
- Enable MSPM0 MCAN
Interrupts: the MCAN module provides different interrupt sources which
can be configured to source a CPU interrupt event. In order of
decreasing interrupt priority, the CPU interrupt events from the MCAN
are configured here.