SLOS970B January 2018 – January 2025 TPA6404-Q1
PRODUCTION DATA
The pinout of the TPA6404-Q1 was selected to provide flow through layout with all high-power connections on the right side, and all low-power signals and supply decoupling on left side.
Section 9.4.2 shows the area for the components in the application example (see the Section 9.2 section). This layout example is taken from the EVM PCB.
The TPA6404-Q1 EVM uses a four-layer PCB. The copper thickness was selected as 70 µm to optimize power loss.
The small value of the output filter provides a small size and, in this case, the low height of the inductor enables double sided mounting