SLUSBX9J March 2014 – October 2026 TPS23861
PRODUCTION DATA
Inrush-current limiting is provided by the TPS23861 according to the curve in Figure 7-12. When the port is first powered on, the TSTART timer is started. While the TSTART timer is counting, the port current is limited to IINRUSH, as shown in Figure 7-12. If at the end of tSTART period the current is still limiting at IINRUSH, the port is powered off and the STRTn bit in the Start/ILIM Event Register is set with the option of asserting an interrupt.
Figure 7-12 Foldback During Inrush (at port turn on) IInrush vs VPORT