SLUSFP1B April 2025 – November 2025 UCC34141-Q1
ADVANCE INFORMATION
The maximum output current and output power capability of the VEE buck-boost converter at different VDD-COM and COM-VEE voltages are shown in Figure 7-6 and Figure 7-7. It can also be calculated in the Excel calculator tool, as another design supporting doucment besides this datasheet. The power module has two independent output power capablilities: one is of VDD-COM output as shown by the SOA curves in the Typical Characteristics section, and the other one is of COM-VEE output as shown in this section. Excessive output power requirement out of either of the two output power capablity can cause an output undervoltage protection and shutdown of the device.