SLUUCN4B January 2023 – December 2024
This command returns the cell voltages, PACK voltage, BAT voltage, cell currents, cell powers, power, and average power on ManufacturerBlockAccess() or ManufacturerData().
| Status | Condition |
|---|---|
| Activate | 0x0071 to ManufacturerBlockAccess() or ManufacturerAccess() |
Action: Output 32 bytes of data on ManufacturerBlockAccess() or ManufacturerData() in the following format: aaAAbbBBccCCddDDeeEEffFFggGGhhHHiiIIjjJJkkKKllLLmmMMnnNNooOOppPP where:
| Value | Description | Unit |
|---|---|---|
| AAaa | Cell Voltage 1 | mV |
| BBbb | Cell Voltage 2 | mV |
| CCcc | Cell Voltage 3 | mV |
| DDdd | Cell Voltage 4 | mV |
| EEee | BAT voltage. Voltage at the BAT pin. This is different than Voltage(), which is the sum of all the cell voltages. | mV |
| FFff | PACK voltage. Voltage at the PACK+ pin. | mV |
| GGgg | Cell Current 1. Simultaneous current measured during Cell Voltage 1 measurement | mA |
| HHhh | Cell Current 2. Simultaneous current measured during Cell Voltage 2 measurement | mA |
| IIii | Cell Current 3. Simultaneous current measured during Cell Voltage 3 measurement | mA |
| JJjj | Cell Current 4. Simultaneous current measured during Cell Voltage 4 measurement | mA |
| KKkk | Cell Power 1. Calculated using Cell Voltage1 and Cell Current 1 data | cW |
| LLll | Cell Power 2. Calculated using Cell Voltage2 and Cell Current 2 data | cW |
| MMmm | Cell Power 3. Calculated using Cell Voltage3 and Cell Current 3 data | cW |
| NNnn | Cell Power 4. Calculated using Cell Voltage4 and Cell Current 4 data | cW |
| OOoo | Power calculated by Voltage() × Current() | cW |
| PPpp | Average Power | cW |