If [SOC_CHARGE] in
Charging Configuration is
set while
[V_SOC_CHARGE] remains 0, then the voltage
threshold control, as described in Section 4.3, is replaced with the RelativeStateOfCharge() control.
With this method, the following
changes in control transitions occur:
- [LV] charging state and
RelativeStateOfCharge() > Charging SOC Mid; move to
[MV] charging state.
- [MV] charging state and
RelativeStateOfCharge() > Charging SOC High; move to
[HV] charging state.
- [MV] charging state, [DSG] = 1,
and RelativeStateOfCharge() < Charging SOC Mid –
Charging SOC Hysteresis; move to [LV] charging state.
- [HV] charging state, [DSG] = 1,
and RelativeStateOfCharge() < Charging SOC High –
Charging SOC Hysteresis; move to [MV] charging state.
Table 4-1 RelativeStateofCharge()
Range
| Class |
Subclass |
Name |
Type |
Min Value |
Max Value |
Default Value |
Unit |
| Advanced Charge Algorithm |
SOC Range |
Charging SOC Mid |
U1 |
0 |
100 |
50 |
% |
| Advanced Charge Algorithm |
SOC Range |
Charging SOC High |
U1 |
0 |
100 |
75 |
% |
| Advanced Charge Algorithm |
SOC Range |
Charging SOC Hysteresis |
U1 |
0 |
100 |
1 |
% |
Note: If the
[V_SOC_CHARGE] = 1, the Voltage or
RSOC(0 Range feature described in
Section 4.3.2 will be used to
determin the state of charging even if
[SOC_CHARGE] = 1.